This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCT8316AEVM: LED3

Part Number: MCT8316AEVM
Other Parts Discussed in Thread: MCT8316A

Hello Team,

Checking with the datasheet of the device the pin39 description is NC together with other pins:

However, checking with the datasheet pin39 is connected to ALARM (LED3), can you share more details about this connection?

Regards,

Renan

  • Hi Renan,

    PIN39 on the RTM version of the MCT8316A is indeed NC. The ALARM LED connection on the MCT8316AEVM is a legacy schematic made on the pre-RTM PMCT8316A. This is not needed or used for the RTM MCT8316A device.

    However, please do note that the ALARM pin function will be added back for the MCT8316B device.

    Regards,
    Eric C.