This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2667: constant (DC) output value

Part Number: DRV2667
Other Parts Discussed in Thread: DRV2700

Hi , can I use this IC to drive constant (DC) output voltage ?

I mean to send some I2C commands to set constant output value (without sending I2C command always)

thanks,

Elimelech. 

  • Hi Elimelech, 

    this isnt possible with the internal signal generator on DRV2667, The minimum frequency is around 7 Hz. 

    for your application using DRV2700 with an external uC/DAC to create a programable DC source is the better option.

    Regards,

    Arthur