This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCF8316A: questions of MCF8316A

Part Number: MCF8316A
Other Parts Discussed in Thread: MCT8316Z,

Dear Team,

I see that they have a new driver (MCF8316A, MCT8316Z), I wonder if it is suitable for precise position control (angle position control), or just for smoother and smoother running of high-speed motors?

Many Thanks,

Jimmy

  • Hi Jimmy,

    Thank you for your question on the Motor Drives E2E Forum.

    MCF8316A and MCT8316Z are not suitable for precise position control but their key value propositions are:

    Ease of use - code-free sensorless motor control

    Low audible noise - PWM modulation, dead time compensation, and variable commutation mode

    Ultra-fast start up - Quick, reliable motor start up from zero speed

    Fast deceleration - 100% to 10% speed reduction within tens of ms

    High efficiency - with various PWM modulation techniques

    Size - Reduce board space up to 70%

    If all of your questions have been addressed and answered please help mark this thread as resolved.

    Best Regards,

    Robert

  • Hi Jimmy,

    If there are no more questions, could you please help mark this thread as resolved?

    I will close the thread for now, but feel free to open it again if you have an additional question around this topic.

     

    Best,

    Robert