Hi,
Have purchased DRV8353RS-EVM. Have to change the speed reference to run motor using Potentiometer R54 on board.
I have installed CCS project, proj_lab05b . Could build and generate .out file.
Since in my application, I need to test a 2 wheeler with this board, speed reference has to be from a potentiometer.
Also Eval board should work wihout GUI in my application - board will be used as a stand alone motor controller with analog speed reference from potentiometer. Power to board will be from 48V battery .
Please guide in making necessary changes in firmware to bypass present speed reference taken from GUI and instead take speed reference from Pot R54 on board. Also any firmware change needed to make the board work without GUI or computer connection.
Regards,
Anil