Hello all,
I am using the MCT8316Z hardware variant to drive a BLDC motor within a mechanical assembly. This assembly applies some friction for the motor to overcome. I am a bit confused as to how to interpret the problem I am having. Basically, I am giving the motor 100% duty cycle to try to get it to overcome the friction and just spin as much as it can. However, the motor simply produces a buzzing sound and the nFault condition is pulled low. I think that it is entering a motor lock condition because all the other conditions seem not to be violated. The current draw is only about 0.7A (well below the Ilimit threshold).
What I am hoping to happen is that the motor simply pulls the current that it needs to overcome the friction of the mechanical assembly. Am I thinking about this correctly?
Any help would be appreciated.