This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8305: BEMF value in DQ reference frame

Expert 1215 points
Part Number: DRV8305

Hi,

I have measured the back emf  waveform between two motor terminals (phases) and it looks like so:

So I have 9V peak-peak (4.5V Amplitude).

It is sine, but in D-Q reference frame it will be constant DC waveform (at a specific speed).

What will be the value of Back EMF in D-Q reference frame?

is it 9/2/sqrt(3) ?

Adam