This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BDC Motor Current Sense Amplifier Using Old Op-Amp and Comparator

Other Parts Discussed in Thread: LM324, LM393, LM339, LM358, INA219, DRV8876, DRV8874, DRV8873

I like to Drive a Brushed DC motor. This is my motor 



I intend to design a low side (or High side if is not possible) shunt based current amplifier circuit. 
Problem is i have to to use combination of old Op-Amps and Comparators like: LM324,LM358,LM393,LM339,etc
 I know about benefits of new current shunt amplifiers like ina219 and similar parts and newly design zero drift op-amps. but i limited to use these parts.can anyone help to say which one of these parts can i use or maybe share a schematic. thanks