This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ULC1001-DRV290XEVM: Piezo transducer sourcing

Part Number: ULC1001-DRV290XEVM

Hi,

I'm looking for a source for a piezo transducer to work with the ULC1001-DRV290XEVM demonstration board.

The dimensions mentioned in the application note (22mm OD, 20mm ID, 10mm tall) would be fine to start with.

Are there any suggestions to source these items?

thanks,

Colin