This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8245-Q1: Control ITRIP using DAC

Part Number: DRV8245-Q1

Hi team,

My customer is using DAC to control the ITRIP.

Max current is 6A, RIPRORI is using 3kohm, VIPROPI is 2.77V typ.

Considering ITRIP = ((VITRIP - VDAC) / RIPROPI) X AIPROPI, the ITRIP accuracy will be influenced by AIPRORI error and VITRIP error.

In worst case, actual ITRIP could be > +/- 1A comparing to expected ITRIP.

Do you have any method to improve the ITRIP accuracy?

Best,
Zeming