This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCF8316AEVM: After I press READ EEPROM it disconnects and comes up with this error

Part Number: MCF8316AEVM
Other Parts Discussed in Thread: MCF8316A
Hi,
This's from Taipei, On14 Feb, Asia's T/I customer service need us write this question for Product Engineer.
Order number: T03841800
Date placed:02/08/2023
ITEM:MCF8316AEVM ,  MCF8316A three-phase sensorless FOC BLDC motor driver evaluation module
Type:Tool
Question:
We just received the development board from you, but after working with it for just 1 day, it's not working any more.
I can connect to the target, (hardware connected) but I can not read or write to the boards EEPROM. It comes up with an error and disconnects.
Can you let me know where I can get support on this matter please.
*COM3:9600 Hardware connected.
*There is an issue with the device connectivity.ple reastart the GUI.
*After I press READ EEPROM it disconnects and comes up with this error.
We are in Taipei.
Regards
Lisa 
  • Hi Lisa,

    Thanks for your question on the Motor Drives E2E Forum. 

    Have you been using the guided tuning steps on the GUI, the User's Guide, and the MCF8316A tuning guide?

    Another thing you could try is not enabling the Auto Read Motor Status. 

    Turning on and off the power supply during the guided tuning may also result in the connectivity issues requiring a restart of the GUI. 

    Best,

    Robert

  • Hi Robert  

    Thanks for getting back to me.
    Yes, I have used the GUI and the tuning steps and everything has been working for the first few hours. Things do crash now and again, but I guess that's to be expected.
    Its not working with or without Auto Read Motor Status.
    I have reset everything and turned on the power supply / USB in different order, and restated the GUI a bunch of times, and also tried on Chrome and Firefox - on 2 different computers. Same problem.
    I think there is something wrong with the board.Can you have someone replace the board here in Taiwan or test what I have on hand?

    Best,

    Jonas Lillie 

  • Hi Jonas, 

    To assess the device integrity, please help by providing the following information.

    How much voltage is being applied the EVM?

    What is the current draw by the EVM at 12V?

    Best,

    Robert

  • The voltage is 24V
    Current draw at 12V is 28mA
    FYI, D6 is on D7 is off

    Jonas

  • Hi Jonas,

    The current draw you are recording is about as expected which leads me to believe that the EVM is still in good condition. 

    The firmware actually only uses one LED and that is toggled whenever there is a UART transaction between the PC and the MSP.

    Does the GUI connect first with D6 slowly blinking and then you get the disconnect issue as soon as you do a read or write?

    This may mean that the I2C communication failed between the MSP and the MCF8316A. D6 slow blinks about every half second because the PC periodically pings the MSP to make sure the USB is still connected.

    If this is the case, you may be using the incorrect I2C target address. In the GUI side panel, there is a I2C target address field that is used by the GUI to send commands to the MCF8316. Can you make sure that the GUI is targeting the same address as what is configured in the MCF8316 EEPROM?

    You can click the "Find Address" button to check what address the MCF8316A is configured to.

    Best,

    Robert

  • Yes, D6 blinks slowly, and then when I press "Read All registers" it quickly blinks 3 times, and turns off.
    If I click "Find Address" and try to "Connect to hardware", you can see what happens in the video. It does go through all addresses in the "I2C Target Address", but fails in the end.

  • Any feedback on this?

  • Hi Jonas,

    Is the device being powered by a power supply during these faults? If so, I may need some additional time to debug your issue.

    Let me know.

    Robert

  • Yes, its connected to a power supply

  • Hi Jonas,

    Can you try to reload the GUI and power cycle the MCF8316. Then before reading anything, click the Find Address button.

    Sometimes when the I2C error occurs, the GUI needs to be fully refreshed. The error could be because the target address was changed in the EEPROM so you will need to make sure the matching address is configured in the GUI before read/write for the first time after launching.

    Best,

    Robert

  • Hi Jonas,

    If there are no more questions, could you please help mark this thread as resolved?

    I will close the thread for now, but feel free to open it again if you have an additional question around this topic.

     

    Best,

    Robert