This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8243H-Q1EVM: DRV8243H-Q1EVM

Part Number: DRV8243H-Q1EVM


Is the rising edge of nFAULT only a sure indication for a ClearFault or also for a wake up during the NSLEEP pulse?
The reason for the question is to minimize the time for the NSLEEP pulse, which is stated as 20µs to 40µs.

B.R. Norbert Hoerst 

  • Hello!

    I am not sure I understand the question.  Are you referring to Treset in the datasheet?  That is a max. pulse time of 20us to reset.  But this time can be anywhere between 5us - 20us for the nFAULT to rise acknowledging a reset has occurred.  

    Once nFAULT rises and acknowledges, the nSLEEP pin can be taken back high.

    Regards,

    Ryan