This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8302: What is the maximum high and low level transition frequency of the gate of this IC?

Part Number: DRV8302
Other Parts Discussed in Thread: DRV8301,

Hi team,

The customer is wondering what is the maximum frequency at which the gate high and low level transitions of the DRV8301/8302 outputs can be made? Is it based on f_gate 200kHz(MAX) in datasheet 6.3 or on the time of each action in section 6.6? 

Could you help look into this case? Thanks.

Best Regards,

Cherry