Hello
We are using DRV8256E to drive one of the valve (uses DC Motor).
There are 4 such valves in system, all of them driven by above HBridge
Interestingly the valves that are away (physically) from HBridge circuit operate without issues but the ones near HBridge (physical in wiring) do not operate at all
Even when the PWM is provided to the EN pin there is no M+ or M- signal
Above problem disappears when long wire is added between Valve and HBridge outputs
Other way when a series resistor of 300mOhm is added in this case also the problem disappears
Can anybody please explain me what is happening with this HBridge DC Motor driving scenario.
Valve is 24V, 2.4W
PWM and DIR are given from an Automotive ECU
Power supply is benchtop regulated power supply (24V) + DC DC converter (to power 12V ECU)
Thanks in advance.