Hi,
As far as the data sheet of DRV10964 is concerned, it is possible to adjust the motor start-up time by applying voltage to the CONFIG pin. By changing the voltage division ratio with resistors and changing the applied voltage, the motor start-up time is shortened to 1600ms. What should I do if I want to further shorten the motor startup time and drive it in about 100ms? Do you have any advice for me?
Thanks,