Looking to try to change design to from DRV8432 (apparently suddenly withdrawn from all documentation and distributors).
First a question on the speed of the current sense output - do you have any documentation on the bandwidth - for example would it be able to show the current with a 1 uS on time (low duty cycle PWM)? Does it show both positive and negative currents (i.e. regen) or only positive currents (must look at both sides to get sign)? The circuitry in the LMD18200T was not sufficiently fast for an accurate reading for such a duty cycle.
Data sheet is preliminary. It seems questionable that each output is given 3 pins to handle the current while the ground pin associated with these same channels have only a single pin per channel which would be carrying up to 10A. I would think that two pins for the output and two for the associated ground would more easily allow the per channel grounds to have appropriately sized traces and package pins for the higher currents. They are adjacent so this is just a documentation and wire bonding change. It would allow much wider traces to handle the current levels these devices are describing. The Vin appear to be internally bussed, so the 4 power pins should be able to share the current - especially when driving motors where not all outputs are simultaneously sourcing current.
Do these parts handle short circuits without the need for the external inductor needed on the DRV8432 (needed to slow the current rise so the current limit circuitry had time to operate)?
When bridging the outputs (effectively parallel for higher current), what values of series inductance are suggested to handle the skew in output timing?
Does an over current on one channel set the common fault to disable all four channels (i.e. safely turning off any bridged outputs)?
I'm looking forward to the release of these new drivers. My use is as part of a servo drive: voice coil, 2-phase, and 3-phase. The step motor current control modes do not work in these applications, so the pure PWM input driver is greatly needed. No warning was given on the termination of the DRV8432 and there is a feeling that the previous long lead orders for this part may not be honored, given the complete removal of all data sheets and references from TI and from distributors within 48 hours!
Thanks