This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[DS GLOBAL] Request for recommending Motor Driver IC

Other Parts Discussed in Thread: DRV8825, DRV8426

Hi, TI support team

I have received an inquiry from a customer to recommend a product with the specifications below.

1. Motor type: UNIPOLAR STEP MOTOR (if there is no UNIPOLAR type, BIPOLAR is also available)

2. STEP: Products that can be used up to MICRO STEP

3, voltage: typical +24V

4. Current : MAX 2A or 3A

5. Application : Printer

Thanks.

Regards,

MJ