Hi,
In DRV8412 datasheet it states that OC current threshold can be set by resistor values according to table 2. I guess it is assumed that inductors are placed in series with MOSFETs outputs, right? I did some OC testing on the eval board with inductors replaced by the recommended power ferrite beads. My measurement shows that the OC threshold is as high as 12A even with default 47K resistor. I guess with power ferrite beads the chip must be used in OC latching mode since OC threshold cannot be set lower. can anyone advise on this? can anyone share more data with power ferrite beads? thanks.
Best regards
Gordon