This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8833C: Microstepping with DRV8833C

Part Number: DRV8833C


Hi,

I'm evaluating the DRV8833C for use with our stepper motors.  Section 8.2.21 of the spec sheet states:

The DRV8833C can support full- and half-stepping modes using the PWM interface

Does this mean that the DRV8833C does not support 1/8 (n = 8) and other microstepping levels?

Thanks!
Matt

  • Matt,

    Does this mean that the DRV8833C does not support 1/8 (n = 8) and other microstepping levels?

    Correct. The DRV8833C does not have an integrated step indexer to support higher stepping rates. If you require higher stepping rates, I recommend the DR8411A which has a dedicated VREF pin to adjust the motor current. A DAC can be connected to VREF with a sinusoidal output to generate the desired microstepping rate.

    Regards,

    Pablo Armet