Hello,
I've designed a custom board with the DRV8844. This is the first time i'm using this IC and I need help in reviewing and cross checking the schematic. I can send the schematic image as a private message. Please help me regarding the same. Also i have a few queries,
1) Since the IC is also capable of driving stepper motors, i've assumed it can accept standard PWM inputs on all INx pins from a 3.3V logic micro controller.
2) In case one of the HS or LS mosfets inside the IC burns, how can we know ? and what can we do to perform a smooth cut off ?
3) What else can i add to help in protecting the drive circuitry from spikes generated by solenoid ?
If any other info is required from my side, please feel free.
Thanks,
Badri