This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV3245Q-Q1: dose SPx and SNx of DRV3245 support both positive and negative current sampling?

Part Number: DRV3245Q-Q1

Hi team, please refer to the below picture, customer want to place current sense resistor on the phase, whose current is positive and negative, so the input voltage between SPx  and SNx is positive and negative.  according to the absolute maximum rating, Although SPx and SNx, SOx can stand negative voltage, from where I am standing, it represent that the device isn't broken in the range (-2~5.5V, -0.3~VREF+0.5V ), but the SOx cannot output negative voltage and amplifier cannot work when SPx and SNx input negative voltage, right?