Hello,
I would like to use MCT8315A with full stand-alone mode. I saw in the datasheet :
"Register settings can be stored in non-volatile EEPROM, which allows the device to operate stand-alone once it has been configured.
The device receives a speed command through a PWM input, analog voltage, frequency input or I2C command."
My question is : it's possible to write in EEPROM a fixed speed value because I would like to start motor when VM is switch on without external command. Can you tell me which register is used t?
Best Regards
Franck