Other Parts Discussed in Thread: L293D, DRV8830, TPS54310, DRV8833
Could any one recommend H-bridge for motor control? There are many available modules, but I haven't found an ideal one:
I don't need very large current, so 600mA is enough, which is satisfied by L293D. L293D also has the smallest footprint among the four. However, I need only two outputs, satisfied by TA7257P, and L293D has two redundant pins here.
Could anyone recommend a H-bridge that meets most closely the demands?
And does there exist any "H-bridge" selection tool so one can quickly found the best match?