Other Parts Discussed in Thread: MCF8316A
Hello Team,
currently I am selecting a intergrated brushless motor driver chip , and the requirement is that the size should be small and the working current should be as large as possible. We selected MCT8316A1VRGFR, and I would like to ask:
1. Is this one recommended for new design?
2. If it is recommended, I think this is a non-inductive FOC vector control, using register to do vector control. If we directly use this chip, does the register have a default configuration?
3. The peak current of this new film is 8A. How much continuous current can support? It's not in this specification.
4. Does this chip only support FOC vector control? How about square wave control?
thanks !