Hello,
I'd like to confirm the value of RREF1 and RREF2 how those are connected. It is mentioned like this in table 7-1.
On the other hand, the typical application schematic shows in series like this. Would you please tell me if the above comments in Table 7-1 is correct even though the typical application shows those are connected in series like this? I mean the value in table 7-1 defines <50kOhm at parallel combination, but those should be connected in series, so it confuses my customer.
Best Regards,
Yoshikazu Kawasaki