This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8251A: The OCP test

Part Number: DRV8251A

Hi team,

My customer wants to have a test on OCP performance and they add a sliding resistor to change the load to enter OCP status,

But actually they are not sure the protection they catched is OCP or OTP. Do u have any advice on distinguishing OCP or OTP? 

And do u have any advice on the OCP test? 

  • Zoey,

    They can check the RETRY time by monitoring the outputs.  If outputs disable and re-enable every 3ms in a very consistent manner, then it is OCP.  OTP will also disable the outputs, but recovery will be more variable as it depends on the hysteresis of the temperature sensor.

    Regards,

    Ryan