Other Parts Discussed in Thread: LM5113
Does this driver support the use of GanFet's or is it only designed for the use of MosFets?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Arturo,
Thank you for your question! The DRV8306 was specifically designed to drive MOSFETs and therefore applies a VGS voltage of around 10V. GaN FETs typically require a lower VGS voltage such as 6V, so the DRV8306 is not suited for driving GaN FETs.
Regards,
Anthony Lodi
Is there a specific integrated chip, with the same functionality, that you recommend for applications using GanFet's? Or do you have a specific combination of BLDC motor controller and drivers that you recommend? I have been using a UCC2626DW and LM5113 pair to run a BLDC Hall Sensor Motor. Getting a consistent reliable performance from this pair has proven difficult. Typically, the LM5113 chip would instantly burn on startup or perform as intended for 15 seconds then burn out. The GanFets were configured in a Half bridge configuration so the GanFet's would burn along with the driver.
Hi Arturo,
What is the bus voltage used? GaN is typically used in applications with high bus voltages such as 220V.
Regards,
Anthony
Hi Arturo,
Thanks for the details! Out of curiosity given that the voltage level is so low, what is the reason behind using GaN FETs instead of MOSFETs?
Regards,
Anthony Lodi
Hi Arturo,
Please let us know if you require further assistance on this debug.
If not, please help mark thread as resolved. Thanks
Best Regards,
Andrew