This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCT8316Z: Current limit does not work

Part Number: MCT8316Z


We are using MCT8316Z and would like to limit the output current to the motor.

we set the Ilim input to 1.25V (AVDD/2-0.4)

and the CSA gain to 1.2V/A

This to my understanding should limit the motor current to 1A.(according to section 8.3.12)

I place a scope on one of the motor phase and can see even 6Amp on the phase (with PWM of 50-60%)

(Not to mention that we burned 4 motors)