This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8889-Q1: Sleep mode with SPI activity

Part Number: DRV8889-Q1

Hello,

if I enter the DRV8889 sleep mode with nSLEEP=0 and have some SPI activity from another device on the same SPI bus as the DRV8889, can it be a problem for the device inputs or not? Because in the datasheet it says: SPI is disabled in sleep mode.

Thank you

Best regards,

lyto