Hi team,
Customer captured a strange waveform as below. CH1 is fault, CH2 is A phase current and CH3 is B phase current. While the A phase current exceed the OCP threshold(1.8A min), the fault pin is pulled low. The strange point is that the fault pin is pulled up later. As you know, the device will remain disabled until either nRESET pin is applied, nSLEEP is toggled low and high, or VMx is removed and re-applied. In above test, those 3 conditions didn't happen but fault is pulled up. Could you please explain it?