Other Parts Discussed in Thread: DRV8316
Hi~ Team.
Customer is looking for 12V/50W BLDC driver solution, so introduced DRV8316-Q1 which peak current is up to 8A.
BTW, DRV8316 datasheet has up to 80W motor application, but DRV8316-Q1 datasheet has up to 40W motor application in first page.
I think both 8316 and Q1 has same die but Q1 has more hard reliability condition.
Can we guarantee DRV8316-Q1 up to 50W application even though described <40W in datasheet?
Let me have advice.
Thanks.