Hello, i need your help. I have to make a project in wich i´ll need to control a bipolar steper motor. I want to have the possibility to obtain full step, half step and so on. So i want to use the DRV8811. The motor i have to use have a nominal voltage = 4,2 Vdc and the driver work with voltages between 8 and 38 V. So my question is, someone knows if i´ll have trouble working in such conditions?
Thank you very much
Houari