Dear TI Team,
We are using a DRV8701E IC for driving a brushed dc motor. Our application involves monitoring motor currents if any shoot is observed during any obstruction to the motor.
We are driving this motor with PWM of 25 KHz .Mosfet used for H-BRIDGE Circuit is IRF1010N N-CHANNEL MOSFET.
We need suggestions for the current measurement from DRV8701E IC.
The Microcontroller adc used is reading from SO (Pin no 11) of DRV8701E IC.
We have kept
reference voltage vref 3 V ,
R-sense shunt resistor = 50 mOHMS
I chop (CHOPPING CURRENT) = 3 Amp.
It is observed while reading the voltage from SO (Pin no 11) of DRV8701E IC.
The output read is found to be not linear compared to current flowing through motors.
How can we read out this current?Do we need to read this value in different way or different algorithm to read the current.