This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8908-Q1: Can this part achieve stall detection?

Part Number: DRV8908-Q1


Hi team,

Customer is using DRV8908-Q1 for auto mirror adjustment, and OEM request to add stall detection function. However, the nominal current is ~150mA, and during stall the current rises to ~700mA. So the OCP or TSD will not be tripped. Do you see any HW or SW workaround to achieve stall detection?

Thank you

Scarlett