This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8711: Coil measurement

Part Number: DRV8711


Hi Team,

I need help with the question below:

If A1HS and A2LS are enabled and the MOSFETs are energized what should be measured across the Coil A.

This part is used as a driver for a stepper motor with the VM is set to 24 VDC
Thank you in advance
Regards,
Marvin