Hi team,
What should the overall steps be for the DRV10987 to develop software in its own circuit environment without the use of an EVM and GUI?
Step 1: It still need to determine the motor related parameters: Some of the parameters are taken from the manual and the other one needs to be measured in real terms?
Step 2: write the values for the registers 0x90–0x96 EEPROM according to the parameters
Step 3: map the shadow registers
Step 4: Fourth, set 0x30 to set the speed
Step 5: read 0x01 speed feedback
Step 6: the motor spins
Is it possible to drive the motor by following the above steps? Could you help check this case? Thanks.
Best Regards,
Cherry