Our customer is considering to use DRV8305NEPHPRQ1.
When they checked the current waveform flowing through PVDD (PIN41) in customer product state, there was a spike current with a peak value of 190mA and a period of about 130us as shown below.
When ENABLE=Hi, a spike current occurs. In the image below, the external FET is stopped, SPI communication is also stopped, and the charge pump frequency register setting (VCPH_FREQ) is b'1 = 419kHz to 491kHz.
A 1Ω resistor is added to the PVDD line and the voltage across it is measured.
(1) Is this waveform normal? (Is this the expected behavior?)
(2) What is the source of this spike current?
Please advise us.
Regards,