Hello,
I have finally got my DRV8312 kit, installed all the programs and have got some motor movement.
But then, the motor stopped and i saw :
1. Red led instead of green one on the main board.
2. Power supply current = 0.5A (with 24v)
3. incorrect voltage of other voltages - no 3.3v, no 5v and no 12v
4. The device itself (DRV8312) is really hot on the top and the bottom.
What could be the possible problems in this case? Anyone can recommend something?
Is there a possibility that something wrong with the device and it should be replaced?
Or maybe there is a possibility to bye a new board but only the main card (as we are limited in time)?
thank you very much for help,
have a nice day
Yulya