Hi, TI expert.
The FG side output defect of the DRV11873 applied to the board being delivered to the customer company (A) occurred, so I ask the following question.
Q1) If you look at the Electrical Characteristics of the datasheet, the current for driving is FG pin sink current: Min 5mA.
If you use it with a current lower than Min 5mA, what problems are expected? (Please answer with technical content.)
For reference, DRV11873 is applied to another customer (B) and the board being delivered is applied at about 2mA, but it is still in use without any defects.
Q2) A pull-up resistor (100K) is applied to the motor FG side output line (12V).In the case of a non-defective sample, 12V level and normal pulse are normally output.
However, when analyzing the FG-side defective output sample, the FG waveform is output, but it is output at a low voltage level (7V to 10V) instead of 12V, and there are also defective samples in which the FG pulse is not
output.
I am using the FG side current as 11mA. What could be the cause of the output voltage drop as above?
Q3) Is there a history of the same problems and defects as above in the past?
Can you provide a technical explanation on how to improve?
If you have related technical data, may I request you to provide them?
(DRV11873) Good sample and bad sample analysis data.xlsx
Please give a detailed explanation if possible.
Thank you.