Other Parts Discussed in Thread: DRV8312
HI ,
i am using the DRV8312 to drive a motor of maxon EC20 9V, 5W. however the motor EC20 supply is only 12V.
However in the datsheet ,it states that the PVDD need to be about 50V.
hence can this driver be used to perform the normal operation and deliver up to 3.5A?
pse advise
Thank you
Regards
jeffrey