This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCT8316Z: duty cycle of the PWM pin

Part Number: MCT8316Z

Hi Team,

May I know does the pwm pin of MCT8316Z able to be set to a high level as a duty cycle of 100%?

Best regards,

Annie

  • Hi Annie,

    Thanks for your question on the motor drives E2E forum. 

    The MCT8316Z device consists of an integrated 100-mΩ (combined high-side and low-side FET's on-state resistance) NMOS FETs connected in a three-phase bridge configuration. A doubler charge pump provides the proper gate-bias voltage to the high-side NMOS FET's across a wide operating-voltage range in addition to providing 100% duty-cycle support. An internal linear regulator provides the gate-bias voltage for the low-side MOSFETs. The device has three VM motor power-supply pins which are to be connected together to the motor-supply voltage.

    Let me know if this answers your question!

    Best,

    Robert

  • Hi Annie,

    If there are no more questions, could you please help mark this thread as resolved?

    I will close the thread for now, but feel free to open it again if you have an additional question around this topic.

     

    Best,

    Robert