This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCT8316Z: How the dual charge pump works

Part Number: MCT8316Z


Hi Team,

The customer wants to know how to drive with two charge pumps.

Thanks,

Annie

  • Hi Annie,

    Thanks for your question on the Motor Drives E2E Forum. 

    Why is customer trying to drive with two charge pumps? What is the performance they are trying to get out of the driver?

    Best,

    Robert

  • Hi Annie,

    Here is the datasheet description on the output power stage: 

    The MCT8316Z device consists of an integrated 100-mΩ (combined high-side and low-side FET's on-state resistance) NMOS FETs connected in a three-phase bridge configuration. A doubler charge pump provides the proper gate-bias voltage to the high-side NMOS FET's across a wide operating-voltage range in addition to providing 100% duty-cycle support. An internal linear regulator provides the gate-bias voltage for the low-side MOSFETs. The device has three VM motor power-supply pins which are to be connected together to the motor-supply voltage.

    Hope this helps.

    Best,

    Robert

  • Hi Annie,

    If there are no more questions, could you please help mark this thread as resolved?

    I will close the thread for now, but feel free to open it again if you have an additional question around this topic.

     

    Best,

    Robert