Hi team,
The MAX_speed register in the datasheet is defined as follows:
How does the value of MAX_speed scale to the actual speed of the motor (assuming units r/min)? Is the value of MAX_speed the target speed of the motor? For example, set MAX_speed = 100, is the motor speed 100 r/min?
Could you help check this case? Thanks.
Best Regards,
Cherry