This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8462: Is it possible to drive a bipolair 3-phase stepper motor?

Part Number: DRV8462
Other Parts Discussed in Thread: DRV8962

Hi all, 

I'm just wondering if it is possible to drive a 3-phase bipolair stepper motor with the "DRV8462" driver. 
When i'm looking to the two full H-bridge configurations i would say: Yes it's is possible. You only need 3 half bridges for 3-phases.
But I have no idea if it is possible with the digital core of the "DRV8462".