This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8703-Q1: DRV8703-Q1 avoid OCP with unused half bridge

Part Number: DRV8703-Q1


Hello,

For DRV8703-Q1, if the OUT2 half bridge is not used and just left THE ghx/glx Pins  float, how to avoid the OCP warning? Setting the DIS_Hx_VDS and DIS_Lx_VDS bit to 0 in VDS control register and prevent the driver stopping,  but the OCP bit in Fault status register will still set. This will trigger the MCU stop PWM at another half bridge. How can avoid this OCP fault warning?