Part Number: DRV8842
Other Parts Discussed in Thread: DRV8840,
Dear Specialists,
My customer is evaluating DRV8840 and DRV8842, they have a question about nFAULT.
I would be grateful if you could advise.
---
Some VM devices have nFAULT going low when a voltage 1V is supplied.
Could you please advise the condition of VM voltage that nFAULT becomes L.
According to the datasheet, the operating voltage of VM is MIN: 8.2V ~ MAX: 45V.
On the other hand, the VM undervoltage lockout voltage is TYP: 7.8V ~ MAX: 8.2V.
*I thought that the motor driver would not be able to pull nFAULT low (do not operate) if it was about 1V.
Is there a possibility nFAULT becomes L at VM1V ?
System behavior
After turning on the power to the device, the power (3.3V system) that controls the signal of the CONTROL system of the motor driver is turned on immediately.
・nFAULT is connected to CPLD and pulled up to 3.3V system by CPLD (several tens to hundreds of kΩ).
・24V is supplied to VM at a certain timing after powering on the equipment, but until then a low voltage of about 1 to 1.1V is supplied to VM.
---
I appreciate your great help in advance.
Best regards,
Shinichi