This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCT8316Z: MCT8316Z brake function not available

Part Number: MCT8316Z
Other Parts Discussed in Thread: MCF8316A

I use MCT8316ZR to control the motor to lift and lower objects. At present, MCT8316ZR can control the rotation of the motor and drive the lifting of objects normally.

I am debugging the MCT8316ZR brake function, but I found that the brake function cannot maintain the motor hovering state.

I have made the following settings for MCT8316ZR:

Control_Register_1 = 0x03

Control_Register_2 = 0x66

Control_Register_3 = 0x46

Control_Register_6 = 0x01

Control_Register_8 = 0x03

Control_Register_7 = 0x03 (this reg set to 0x01 or 0x03 , I feel the same effect)

and set the brake pin to high , drvoff pin to low  nsleep pin to low .


Other registers use default values.

When I need brake enable, the motor can be suspended. Pulling up the brake pin has a slight effect, but it is not very obvious. The braking force is very small.

May I ask what the reason is?

The attachment is a circuit schematic diagram.

Thank you.