This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] DRV89xx-Q1 PWM FFh settings behaivior

Other Parts Discussed in Thread: DRV8910-Q1, DRV8904-Q1, DRV8906-Q1, DRV8908-Q1, DRV8912-Q1

DRV89xx-Q1 (DRV8904-Q1,DRV8906-Q1,DRV8908-Q1, DRV8910-Q1, DRV8912-Q1) device has internal PWM generator. When PWM Duty is set as FFh(max), it is very close to 100% but there is a small gap.

For example. With100Hz: PWM=FFh : ON DUTY = 9.98ms/10ms     = 99.8%

Workaround is to switch to "Continuous mode" then Duty will be 100% ON

Details are attached.

DRV89xxQ1_PWM_Duty.pptx