Other Parts Discussed in Thread: MCF8316A, MCF8315A
Hello,
If I disable both auto read in the GUI I can read all the parameters as well as write new values into the registers. When I activate auto read the motor stops after a few seconds of spinning. The GUI then shows that it is in the MPET KE_MEASURE state. It is not possible to leave this state. In addition, no error messages are displayed. The power supply must be disconnected so that the motor can be rotated again. Now the question is if you have a solution for this problem, and if my board is broken or if I am doing something wrong.
Thanks for the help.