Hi team,
Order number: T04194332
Part number: MCF8316A1VRGFR
Order quantity: 5pcs.
According to the feedback from the customer, this chip cannot be soldered.
Apply a flux to the board, use heat to blow the air, and adjust the temperature to 250 degrees. In this case, the chip will automatically reset and straighten, but the customer has failed. The soldering temperature is not specified in the specification. There is no apparent oxidation problem seen at the pins.
Could you help check this case? Thanks.
Best Regards,
Cherry