This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2700: DRV2700 can output 0 to 150V / 20mA

Part Number: DRV2700

Hello,

My customer is looking for a piezo driver to meet the following requirements.
Does DRV2700 can output 0 to 150V, not +/-100V?
Vin = 0V to 10V
Vout = 0 to 150V
Iout = 20mA (max)

Best regards,

K.Hirano

  • Hi Hirano-san,

    The DRV2700 can output either 0 to 105 V or +/-100 V. If you would like to output 0 to 150 V, you can look at the DRV2700EVM-HV500 which can output 0 to 500 V. The DRV2700 max input voltage is 5.5 V which is the highest input voltage we currently have for piezo drivers.

    Regards,

    Sydney Northcutt